Post Go back to editing

LTspice 26.0 Current not found for .meas OK in viewver

Thread Summary

The user encountered an issue where the .meas command failed to measure the current through a MOV (U9:A) in a circuit simulation, despite the current displaying correctly. The final answer identified this as a regression bug affecting the use of pin names in .meas expressions, which will be fixed in the next release. The workaround is to use port names instead (e.g., 'Ix(U9:1)'). The problem was further confirmed to occur when the symbol PinNames differ from those in the .lib file, even though the simulation runs correctly.
AI Generated Content
Category: Software
Software Version: 26.0.0

Hello,

I have a circuit that includes a MOV from the library.
I am able to display the current through the MOV (Ix(U9:A)), but I get an error when I try to measure it using a .meas expression.


Current_Meas.net(27): Current not found.
.meas TRAN I_MAX MAX Ix(U9:A)
Current_Meas.zip

The settings in Save Defaults are configured to save both device currents and subcircuit currents.

Do you have any idea what could be causing this issue?

Thank you,
Emilien

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.