Post Go back to editing

LTSpice Version Differences

Thread Summary

The user encountered inconsistent temperature sweep results between LTspice 24.0.12 and 26.0.1. The issue was resolved by using the recommended syntax '.step temp -55 125 10' to step the temperature from -55°C to 125°C in 10°C increments. The user also provided a ZIP file with the circuit for further review.
AI Generated Content
Category: Software
Product Number: LTspice
Software Version: 24.0.12 and 26.0.1

Hello,

I am seeing different results with the same .asc circuit in different LTspice versions:

LTspice 24.0.12: V(ntc) changes with temperature and the comparator output switches at a threshold (as expected).

LTspice 26.0.1: V(ntc) and the computed NTC resistance look almost constant (flat plot), so V(out) does not change.

What is the recommended way to make this temperature sweep consistent across versions?

Best regards,

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.