Hi LTSpice won't work on my brand new windows 11 pro machine. Program installs correctly and when I select LTspice updates it works and says "up to date" but when I try to start it even using "run as administrator nothing happens and I get no error message at all. Checking on Task manager there is no LTSpice active or even running in the background it's as if it just doesn't start or crashes upon start with no error messages.
I tried downloading regular LTSpice for windows 11 and even the one at https://LTspice.analog.com/download/24.1.10_test/LTspice64.msi instaling then running msiexec /i "<Path to>\LTspice64.msi" /L*v "<Path to>\MyAppInstall.log etc all to no avail. Ironically we purchased this 5.3GHz 18 core latest and greatest mostly for LTSpice which is the only app that won't work. We have downloaded other apps like Altium and acrobat reader, Google Chrome, Firefox and they all work flawlessly so it's definitely an LTSpice coding issue. Have spent many hours on this and so have the HP software experts.
We are an ADI design partner and really need some support here thanks. Best Steve Smith