Post Go back to editing

LTSpice parallel LC simulation

Category: Software

 I am trying to simulate a simple LC circuit in which the components are parallel. I have protected the ground to prevent dissipating RF energy from the tank, with a large resistor. Im firstly a complete electronics newbie so for one i dont understand how nodes work and thats not for lack of trying to understand, and two why if i click different parts of the circuit is the frequency response different i.e the left side wire gives green no response but the right side gives the expected resonance frequency. I am an NMR spectroscopist and work in the Rf regime and am building a new probe but need to get to grips with the basic LC circuit before i can build my more complicated circuit and simulate it. I need help! Also how do i calculate Q, impedance and get an s11 curve from the results there seems to be no understandable resources out there for a complete beginner!! 

Parents
  • Hello Imogen, 

    here's an answer to some of your questions:

    why if i click different parts of the circuit is the frequency response different i.e the left side wire gives green no response but the right side gives the expected resonance frequency

    If you click on a node in AC-simulation you see the frequency behaviour of that node voltage. On the left side, the voltage does not depend on frequency, cause you force a voltage of constant amlitude 1V and constant phase 0° with the ideal voltage source V1. So it has to show 0dB and 0° at all frequencies. On the right side you see the frequency behaviour of your LC circuit as it forms a complex voltage divider with R1. 

    Also how do i calculate Q

    measure the width Δf of the resonance peak with two cursors a calculate Q=f_res/Δf. In your simulation the shape of the resonance seems distorted due to the limited number of data points (100 per decade). The dip will go further down (and Δf will be smaller) if you use e.g. 500 points per decade.

    Finally in your simulation Q may be very high, as you simulate most probably with ideal L and ideal C. In real world the parasitics of your components may limit Q. If you know parasitics of your components, you should include them into the simulation, otherwise the simulated Q may not be very meaningfull. 

    impedance

    as the complete current through L||C flows also through R1, you may plot the ratio of (V(n001)-V(n002))/I(R1)

    s11 curve

    I think s-parameters make only sense, if you operate (or simulate) your network with some characteristic impedance. (not, if you drive it with an ideal voltage source with impedance 0). 

    there seems to be no understandable resources out there for a complete beginner!! 

    You may start with a Google search like "LTSpice tutorial beginner"

    best regards

    Achim 

Reply
  • Hello Imogen, 

    here's an answer to some of your questions:

    why if i click different parts of the circuit is the frequency response different i.e the left side wire gives green no response but the right side gives the expected resonance frequency

    If you click on a node in AC-simulation you see the frequency behaviour of that node voltage. On the left side, the voltage does not depend on frequency, cause you force a voltage of constant amlitude 1V and constant phase 0° with the ideal voltage source V1. So it has to show 0dB and 0° at all frequencies. On the right side you see the frequency behaviour of your LC circuit as it forms a complex voltage divider with R1. 

    Also how do i calculate Q

    measure the width Δf of the resonance peak with two cursors a calculate Q=f_res/Δf. In your simulation the shape of the resonance seems distorted due to the limited number of data points (100 per decade). The dip will go further down (and Δf will be smaller) if you use e.g. 500 points per decade.

    Finally in your simulation Q may be very high, as you simulate most probably with ideal L and ideal C. In real world the parasitics of your components may limit Q. If you know parasitics of your components, you should include them into the simulation, otherwise the simulated Q may not be very meaningfull. 

    impedance

    as the complete current through L||C flows also through R1, you may plot the ratio of (V(n001)-V(n002))/I(R1)

    s11 curve

    I think s-parameters make only sense, if you operate (or simulate) your network with some characteristic impedance. (not, if you drive it with an ideal voltage source with impedance 0). 

    there seems to be no understandable resources out there for a complete beginner!! 

    You may start with a Google search like "LTSpice tutorial beginner"

    best regards

    Achim 

Children
No Data