Post Go back to editing

Bode analysis of IBB using LTSpice

Thread Summary

The user is facing issues with extracting the Bode plot for an Inverting Buck Boost (IBB) converter using the LT3845 controller in LTSpice. The error encountered is due to a grounded terminal in the FRA component without a specified refnode or associated FRAPROBE. The final answer suggests placing the FRA component correctly in the feedback loop and using the FRAPROBE for accurate measurements. The user also noted that the RHPZ is around 8kHz and that adding an RC series at Vc had no effect.
AI Generated Content
Category: Software
Software Version: 26.0.1

Hello everyone,

I'm currently designing and simulating an Inverting Buck Boost (IBB) converter using a LT3845 controller. Right now I'm working on extracting the Bode plot to ensure the converter is stable and the RHPZ effect is kept at bay, but I'm facing some technical difficulties in using LTSpice's FRA component here. Following the tips in [AN-2579](https://www.analog.com/en/resources/app-notes/an-2579.html) I tried placing the .FRA component, where the signal is injected, in the lower leg of the feedback loop but got the following error (which, to be honest, I have no idea what is suggesting me to do):

FRA Instance @1 has a grounded terminal, with no refnode specified or an associated fraprobe device.

Do you have any tip to correctly perform this kind of measurement using LTSpice?

Thanks in advance.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.