Post Go back to editing

About LTC7803 spice model

Category: Software
Product Number: LTC7803
Software Version: LTspice Version 24.1.4

Hello Support Team,


I am currently evaluating a design using the LTC7803. In the datasheet, the absolute maximum rating for the ITH pin is specified as –0.3 V to 2 V.

However, when I run a simulation in LTspice using the example circuit, the waveform at the ITH pin exceeds 2 V.


Is this an issue with the LTspice model, or will the actual device also exceed 2 V on the ITH pin? If so, does that imply that the datasheet specification is incorrect?

I am currently using LTspice version 24.1.4, and the change log for the LTC7803 model is as follows:
“09/27/25 LTC7803 Updated control loop parameters to improve dynamic response”

I look forward to your response.

Best Regards,

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.