Hello, I am attempting to measure the bode plot for a full-bridge topology in LTSpice using the fra tool, and I am getting results that indicate the phase margin is not found, and that it fails to find the 0dB point. I have the fra inserted in the feedback/compensation loop in series with the output as it would normally be for an actual bode plot. I used the fra wizard to properly set it up, as I am analyzing someone else's design so I do not have all the details regarding the loop bandwidth, but the switching frequency is known. Here are some details to the setup (switching frequency is approx..414kHz):
start frequency: 625Hz
end frequency: 42kHz
2 points per octave
coarse steps up to frequency: 5kHz
stimulus pp0: 79.68mV
stimulus pp1: 4.98mV
F0: 625Hz
F1: 10kHz
start analysis: 1ms
minimum analysis time: 241.546us
stimulus settling time: 100us

I attached a screenshot; hopefully, this is enough information. Thanks.