Post Go back to editing

IR2110 full bridge gate pulse not proper

Thread Summary

The user is experiencing poor PWM gate pulses in an H-bridge simulation using the IR2110. The final answer suggests that the slow turn-off time due to a high impedance 1 kOhm resistor is causing the issue, and recommends using a faster turn-off path for better performance. The user later added a PNP transistor for fast turn-off but encountered abrupt PWM generation and load current, and could not increase the voltage beyond 35V with the IR2110S, 10uF bootstrap, and SPWM (24kHz).
AI Generated Content
Category: Software
Product Number: LTspice
Software Version: 25

Hi All,

    I want to study the parasitic effect on h-bridge using IR2110 full bridge. In my simulation using modified trapezoidal, it works. But PWM gate pusles are poor. Can u make it work exactly for my study.

ThanksH_IR2110_TEST3.asc

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.