I'm trying to model a resistance that is dependent on frequency for core resistance of a transformer. I couldn't get that to work so I thought I would do something simple. I used LAPLACE=1/R in a G source. A plot of that against a resistor matches so I thought I was in a good place. Then, I created a resistor-inductor-resistor series with my resistor "under test" as being in parallel with the inductor. Now when I run the test, the G-source compared to the standard resistor no longer give the same result as the frequency increases. NOTE: I have not yet introduced any frequency into the G-source equation. It is still just a fraction. also note that this is all with AC simulation. (I'd love to use transient as well but I don't think that would work at all)