Post Go back to editing

DC sweep down-count does not plot results

Category: Software
Software Version: V24.1.10

When using a down-count in a .DC directive, the simulation itself appears to run, but the results cannot be plotted.

In the attached circuit, the sweep in the upward direction behaves correctly:

.dc V2 0 5 0.1


However, when sweeping downward, the data is not plotted and the following message appears in the log:

HystComp.net(11): Corrected wrong sign of increment.
.dc V2 5 0 0.1
^^^^


If I change it to:

.dc V2 5 0 -0.1


the log message disappears, but the results still do not plot.

I tested with older versions and confirmed the following:

V17: both upward and downward sweeps work correctly

V24.1.8: also works correctly

Best regards,
Denspa

251113_HystComp.zip

Parents Reply Children
No Data