Post Go back to editing

Follow-up on TPA3116D2 Simulation in LTspice

Category: Software
Product Number: LTspice
Software Version: 24.1.10

Hello Mathias,

Unfortunately, I have to reach out to you again regarding this topic. I’m now using the latest version of LTspice and trying to simulate the Class D amplifier TPA3116D2. With the alternate solver, the simulation does run, but as mentioned before, I still get unrealistically high output voltages of around 250 V — which obviously cannot be correct.

Previously, the simulation worked fine with version 24.0.12, but now I can’t achieve any reasonable output voltage levels anymore, despite trying several adjustments. Our students are all using the newest LTspice version, and installing an older version is quite difficult to manage.

Do you have any further suggestions or ideas on how to resolve this issue?

Thank you very much for your help!

Best regards,
René

TPA3116D2.LIBTPA3116D2.asytest_amp3.asc

  • Hi  ,

    Without doing anything yet, running with UIC is highly discouraged. I'll take a look.

    mike

  • Dear  ,

    Please accept my appologies for not looking thoroughly enough into this matter. Your case reveales that there is a bug in the entire 24.1 line that causes some dependent sources with POLY(n) to be evaluated incorrectly. The next release will have this corrected. Thanks for insisting!

    Meanwhile, I can offer to just change the TPA3116D2.LIB as workaround. I can't post the file here (for copyright reasons) but the changes are simple:

    Replace line 304 with:
    VEBETA VBETA 0 1.852

    and line 306 with:
    bg1 d s i=v(d,s)*v(g)*v(vbeta)

    and line 435 with:
    BE8 RAMP NET112 v=62.5e-3*v(NET0141)*v(PVCC)

    In addition, don't use the .tran UIC flag. Instead:

    .tran 0 5ms 0 startup

    Run it with the gear integrator and optionally with

    .options itl4=40

    The latter makes the simulation a bit faster.

    However, even with these changes, I don't get a clean sinusoidal signal like on your screenshots. (Neither in 24.1.10, 24.0.12 nor in LTspiceXVII)

    Best Regards,
    Mathias

  • Dear Mathias,

    Thank you very much for your quick and extremely helpful reply.
    I applied the changes you suggested, and the simulation is now working correctly.

    The sinusoidal signal is also fine again — it was just an overdrive issue on my side.

    I’m glad that my case helped uncover a bug in the POLY(n) evaluation.


    Best regards from Switzerland,
    René Grabher

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.