Post Go back to editing

Simulation problem of LT3748

Category: Software
Product Number: LT3748
Software Version: 24.1.10

Vn005 test by Vds

Vn008 test by Vcompensation

Vn010 test by Vgate

In the pic; I model the inductor coupling to flyback transformer, turns ratio 2:1. To achieve stable 15V output voltage working from 0.2w to 2w. But while changing the input voltage like from 50 to 30V, the output has big variation; is there mistake in this simulation or how optimize the circuit to actual circuit closely.

Thank you for your support

Thread Notes

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.