Post Go back to editing

There is more than one sub-circuit definition with this name, which is ill-formed

Thread Summary

The user encountered an error in LTspice after updating, where multiple sub-circuit definitions with the same name cause simulations to fail. The solution is to remove or subjugate duplicate definitions, or add the .options directive 'allow_ambiguous_models=true' to the schematic, though this will still generate a warning. The issue is common with Texas Instruments models, and the duplicates are often identical.
AI Generated Content
Category: Software
Product Number: newest version 24.1.9
Software Version: 24.1.9

There is more than one sub-circuit definition with this name, which is ill-formed.   updated today from older version 17.0.36 i believe.  Now get this error on older simulation that worked.  Someone else post this issue back in January as well.  What is the solution?