Post Go back to editing

Bug report -lt spice asked me to report, not clear how

Category: Software
Product Number: LT spice bug
Software Version: 24.1.9

Hi,

Apologies if this is the wrong place, trying to be helpful and report a recurrent bug, created this account and happy to be pointed to best way to do so.

Using LT spice to simulate a high voltage PSU made of several HF HV AC voltage generators feeding voltage multipliers in parallel, I wanted to simulate the various modules being unsynchronised and non identical.

I could get a solution if all were same frequency and adjusted a fixed phase.\

When I tried different frequencies between them (nominal 10Khz, had small differences of say 10 or 100Hz or bigger say 5kHz) simulation sometimes worked (got expected lf beating with a few with small frequency difference) but tended to close program after a while, sometimes ran very slowly with messages with increasing defcon messages at one point got a fatal error alert saying this is a program fault please report it, so I am trying.

Circuits weren't complex, just a few voltage sources feeding a few stages of voltage multiplier, didn't deliberately try ill-conditioned frequency multiples or phase shifts, problem started pretty quickly with only few supplies of different frequency.  Was using just a sine wave source and tried to run simulation for say 10msec with 10kHz source to give time to stabilise.

Can get a vaguely useful result by assuming all are same frequency and adding random phase offsets manually but was curious to see different frequency effects (like beating, likely magnitude)

  • Hi  ,

    This would be the right place to report a bug. If you could upload your files, we can confirm. Be sure to zip up all schematics, files and symbols.

    LTspice should not have a problem resolving offset signals, as it is pretty easy to produce a beat frequency using sine sources, but it sounds like you have much more going on.

    mike