KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All


Hello,
The circuit you've posted is not valid. The entire right side of the capacitor is floating and has no reference point. In PSpice, for example, this would result in an error — “floating net.” LTspice avoids the error by likely assigning some internal reference to the floating node. The simulation results are actually correct — no current flows, and no filtering occurs — because without a defined path to ground or a load, there's simply no circuit for the capacitor to act upon.
Vilem
What you say makes sense. However I have some followup questions. If I wanted to simulate the following circuit:
If I connect an oscilloscope probe to Vo, wouldn't it be centered at 0V? Also something changed, since on v24.0.8 of LTSpice, the floating node had no DC component.
You're right to ask — this is an important detail that’s easy to overlook.
If you connect an oscilloscope probe to Vo in a real circuit, then yes, the signal will appear centered around 0 V because the probe (with its high input impedance, typically 1–10 MΩ) effectively provides a DC path to ground. That’s what allows the capacitor to block the DC component and the output to “float” to a proper AC-centered signal.
As for LTspice v24.0.8, I'm just a user myself, so I don't know exactly how the developers handled floating nodes in that version. But it seems the simulator may have implicitly assigned some weak reference, giving the appearance of correct DC blocking even without a defined load. In the newer versions, this behavior appears to have become more strict or realistic — if there's no DC path, the node floats as it would in reality.
To replicate real oscilloscope behavior in LTspice, you can add a large resistor (e.g., 10 MΩ) from R3 to ground. This simulates the effect of the oscilloscope's input impedance.
Thats a smar way to simlate it. Thank you
Thats a smar way to simlate it. Thank you