Post Go back to editing

LTC4041 LTSPICE 3/10/25/30F Supercapacitor Behavoir

Category: Hardware
Product Number: LTC4041

Hi All,
I am working on a power protection circuit using the LTC4041. The circuit is supposed to provide backup supply. However, when I simulate the LTC4041 with different capacitors such as 3F/10F/30F, the LTC4041 doesn't work stable (I think I need more time for capacitor charging). SCAP voltage doesn't seem right. But when I run the simulation with 10mF the ltc4041 works as expected.

Questions:

  1. Can anyone check the LTSPICE schematic and review?
  2. If I need more time for capacitor charging, how can I speed up the simulation? The simulation takes too much time.
  3. I didn't want to start another thread, so other question: Can I use 3V supercapacitor with LTC4041? How should I choose the capacitor operating voltage?

Additional Information:

  • Input voltage: 5V
  • Boost voltage: 5V
  • Capacitor charging voltage: 4.59V
  • Total system current: 3.1A
  • PFI threshold: 4.69V
  • Charge current: 1A

Thanks in advance.

Attachments:

  • Schematic
  • Simulation outputs
  • First output LTC4041 schematic with 10mF
  • Second output LTC4041 with 30F (I increased the simulation time)

Edit Notes

Supercapacitor working voltage question added
[edited by: persoentif at 11:11 AM (GMT -4) on 15 Apr 2025]

Thread Notes