Post Go back to editing

max4206 spice model bug

Category: Datasheet/Specs
Product Number: MAX4206

I want to report a bug of max4206 spice model. I downloated the lib file from analog website.
based on datasheet. if Rset is 5M ohm, the Iref should be 10nA, not 100nA. and when Ilog is 10nA, the VLOG1 should be 0V.

However, I found out when I set Rset to 5M ohm, the Iref is set to 100nA in spice mod. Maybe forget to add the 10.

Thread Notes

Parents Reply Children
  • Hi Romain,

    It's not corrected yet.
    It's still shows the model was created on Oct 10,2012, and in version 0

  • Hi  ,  ,  ,

    I do see that   reported this bug. Can you enter a Technical Support request here. You can reference bug 2140.

    mike

  • Hi everybody :

    This is the answer from tech support :

    Hello Romain,  

    I have been in contact with the team to notfiy them of your issue. They will review this and implement a fix in due time. 

    Following this, we will be closing this technical support case. Should you require any additional support in the future, simply open a new technical support ticket and myself and the team will be available to support you.  

    Have a great day!

     Warm regards,

    L*****

    --------------------------------------------------------------------------

    Hi,

    Thanks for the answer but when you do that.

    Because the first report of this dates a long time ago on the forum.

    I’m not default but in due time seems to me very uncertain…

     Thanks for your help.

     Romain

    ----------------------------------------------------------------------------

    Hello Romain, 

    Unfortunately, I am unable to provide a time frame for when this fix will occur. I have forwarded the issue to the relevant team, who will take is under advisement and resolve when possible. 

    My apologies that I can not provide additional information at this time.

     Warm regards,

    L*****

    So we have to wait and see.

    Have a nice day !

    Romain.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.