Post Go back to editing

max4206 spice model bug

Category: Datasheet/Specs
Product Number: MAX4206

I want to report a bug of max4206 spice model. I downloated the lib file from analog website.
based on datasheet. if Rset is 5M ohm, the Iref should be 10nA, not 100nA. and when Ilog is 10nA, the VLOG1 should be 0V.

However, I found out when I set Rset to 5M ohm, the Iref is set to 100nA in spice mod. Maybe forget to add the 10.

Thread Notes

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.