I recently downloaded LTSpice 24.1.5.
I am working on a problem that specifies an input waveform of 177 cos(377)t, where 177V is the peak voltage and 377 rad/s is the angular equivalent of 60 Hz (2*pi*60).
When I run the analysis calculating the source current for the specified load it displays a peak current of 22.3 A vs. a calculated peak value (verified in the answer sheet) of 12.11A.
I entered 60 Hz for the source description: SINE (0 177 60 0 0 0). Note that I am ignoring teh 90 degree shift between Sine and Cosine. Is my SINE statement correct, using a frequency of 60 Hz instead of 377 rad/s?
Also, where can I find definitions of all the parameters associated with a specific function, in this case SINE?
Thanks,
T