Category: Software
Software Version: ver.24.1.5
The simulation results are incorrect when using a PNP transistor. With an input of 1V, the output should be 5V according to the circuit. However, the final result is completely wrong. When I use an NPN transistor with the same parameters, the results are correct.Please refer to the image below for details.Looking forward to your help.