Currently, I am using LTspice 24.0.12 on windows on arm device and aside from the slightly slow simulation speed, it works very well.
However, in the latest 24.1.X version, ARM64 installation has been restricted.
I am curious if this restriction was implemented to support Windows on ARM64 later.
If not, I think there is no reason to block it, as it works well through the Prism emulation layer.
Please do not restrict the installation of the latest version on Windows on ARM devices.
thanks for your support mike.
I complain about the same issue, there is no point in blocking ARM64 based PC straight in the installation process as it worked flawlessly at least in that older versions. Moreover if there were bugs I assume most people using this software would acknowledge they may be caused by the software being emulated through Prism.
I have tried to update but now I have no way to install it back with the updated installer. Could you provide me with a 24.0.12 installer?
Thanks
sorry for the late reply, try this link
Now it works fine again, amazing.
So grateful!
thank you for the link! works great