Post Go back to editing

LTspice model for ADCMP356 input bias high?

Category: Software
Product Number: ADCMP356
Software Version: LTspice Version (x64): 24.0.15

The bias current on the LTspice ADCMP356 model seems rather high. The 356's spec sheet gives a typical input bias current of 10nA at 0.6V and 170nA at 22V. On the LTspice example circuit ADCMP356.asc, the input bias is about 2.43 μA at 0.6V. I would think it should be 10nA.  Am I missing something? If the input bias should be 10nA @ 0.6V, is there a way to fix this on the ? Thanks -JimADCMP356.asc

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.