Post Go back to editing

ADP5075 phase margin(LTspice, EE-SIM)

Category: Hardware
Product Number: ADP5075

Hello.

I have one question. Please tell me.

I am attempting to simulate the phase margin of the ADP5075.

However, I tried with LTspice and EE-sim and it did not work.

I want to chech the phase margin when the load current is 0~-40mA.

EE-SIM will not operate a load of less than 0~-4mA. It operates correctly at all other loads.

I am attaching a sim date and would appreciate your advice.

Best regard.

0728.file.zip

Thread Notes