Post Go back to editing

Frequency response analysis using LTSpice gives strange results on LT8625s

Category: Software
Product Number: LT8625S
Software Version: Latest LTSpice

Doing a simple ltspice simulation with LT8625S example circuit gives me very weird results. I need to simulate in order to test stability with further elements in the control loop (additional LCs) to attenuate ripple, but so far I'm only testing vanilla examples.

I added a FRA block and started simulating to obtain the gain / phase responses of the open loop buck after fiddling in LTPowerCAD for a VIN=12V and Vout=3.3v.

But the phases are weird and all over the place, and don't resemble a typical buck. Gain as well. Even when doing more accurate/lengthy simulations. They don't match LTPowerCAD either (which shows something that makes much more sense).

I used LTPowerCAD's exported design and LTSpices default example. Both show weird responses. It feels like either I'm wrong about where to place .fra block, or the LTSpice model is buggy.

See attached ltspice file and screenshots of LTPowerCAD and LTSpice.

2021.try_ltspice_lt8625s.asc

Edit Notes

Removed bad image (control to loop)
[edited by: yannickb at 7:46 PM (GMT -5) on 8 Feb 2025]

Thread Notes