Post Go back to editing

LTSPICE: When using a single power supply, the AD8041 input bias current is too high.

Category: Software
Product Number: SOFTWARE
Software Version: V24.0.12

Hi all,

When using dual power supply, the input bias current is approximately 1.2uA, which is within the normal range.

When powered by a single 5V supply, the input bias current exceeds 16uA, which is beyond the maximum value specified in the datasheet.

Where is the problem?

thanks

AD8041.asc

Parents Reply Children
No Data