Post Go back to editing

LTSPICE: When using a single power supply, the AD8041 input bias current is too high.

Category: Software
Product Number: SOFTWARE
Software Version: V24.0.12

Hi all,

When using dual power supply, the input bias current is approximately 1.2uA, which is within the normal range.

When powered by a single 5V supply, the input bias current exceeds 16uA, which is beyond the maximum value specified in the datasheet.

Where is the problem?

thanks

AD8041.asc

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.