Post Go back to editing

AD8666 LTSpice model does not seem to match with datasheet

Thread Summary

The user encountered issues with the AD8666 model in LTSpice, where the output saturated at 9V when used as a buffer or in an AC amplifier circuit. The final answer suggests updating the component library to the latest version to resolve the issue. An accompanying answer noted that the model fails when the supply voltage span is less than 10V, suggesting a workaround by setting V+ to 12V and V- to -3V.
AI Generated Content
Category: Software
Product Number: AD8666
Software Version: LTspice 24.0.12

I am using the AD8666 in an audio circuit as a buffer running on 9V. I wanted to simulate the behaviour for a quick sanity check.

The built-in model in LTSpice seems to be flawed, unless I misunderstood the datasheet. Wiring up a simple AC amplifier, biased at 4.5V feeding in a 20mV signal to the non-inverting input only results in saturation where the output is 9V flat.

The input, at non-inverting pin:

The output:

I tried using it as a simple buffer too, but it doesn't work. I did find another post,  AD8666 LTSpice transient analysis failure
 and the model that provided seems to work.

Why is the built-in model not working (I have updated it to the latest version), and is the other model a better model to use (i.e. is it more accurate to the real amp)? If so, why is this not replacing the older model?

Thanks!

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.