KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
MAX809
Production
The MAX803/MAX809/MAX810 are microprocessor (µP) supervisory circuits used to monitor the power supplies in µP and digital systems. They provide excellent...
Datasheet
MAX809 on Analog.com
MAX809S
Obsolete
The MAX803/MAX809/MAX810 are microprocessor (µP) supervisory circuits used to monitor the power supplies in µP and digital systems. They provide excellent...
Datasheet
MAX809S on Analog.com
Dear Analog community,
I try to simulate a MAX809 with LTSpice 24.0.9
With the most simple circuit, it runs but it throws me an error (see log in the attached zip).
However, if I try to simulate a more complex design, simulation is a lot slow.
Can you help with this error ?
Thanks a lot in advance.
Bonjour
Je cherche le fichier pSpice pour le MAX17227AATA+T. Pourriez-vous m’aider s’il vous plaît ?
Merci d’avance.
Hi Lucio10 ,
This forum is for LTspice questions and requests, and you have posted in reply to an unrelated thread.
Although you should post this particular question as a new question in the Power Management forum, I don't believe we usually satisfy Pspice model requests. Sorry I can't help you more.
mike
Hi Pascal06 ,
Yeah, looks like that is not a well-formed model, using some non-physical components to produce the desired results. I'll look into it.
mike
Hi Pascal06 ,
It looks like the model generally performs as the datasheet indicates the part should work, except I think the assertion should be released after 140ms, not 64ms? The errors would be helpful to a modeler to improve the model.
mike
Hello MStokowski
I hope you're doing well ?
Sorry for this late reply.
Indeed, as stated in the datasheet it should be deasserted at 140ms.
If you look at the simulation below (I just used the same model as the one I used in November 2024) it is deasserted at 92.68ms