Post Go back to editing

Parallel LT8638S Problem Simulating in LTspice with >37V input/output. Real or Model?

Category: Hardware
Product Number: LT8638S

In my LTSpice simulation of the model by analog.com LT8638S loses sync signal if Vin goes above 37 V. 

It also loses sync signal if Vc goes to 0, but maybe this is not such a problem(?)

(The whole schematic contains also a high voltage, fixed ratio DCDC, at low frequency the control loop includes this HV DCDC, but there is a fast lane feedback from the LC filter of LT8638Ss in case somebody asked. But high input voltage causes problems in the reference schematics also.) 

I would like to know if only LTSpice model exhibits this (mal)function, or the actual product behaves the same way? Can I get it work well? Can this be solved by 2 external clocks out of phase?

And overall: can this part be used to generate output voltage close to Vin, if Vin is close to absolute maximum? 

Edit Notes

Expanded Title; added keywords
[edited by: MStokowski at 11:12 PM (GMT -5) on 18 Nov 2024]

Thread Notes

Parents Reply
  • Hi  ,

    That does look like a model problem. I'll report it.

    Some other things I noticed. At 37.5V, the clock signal will run for a couple of cycles at 37.5V, then stop. At other , lower Vin, it's just a messy signal, as shown in the pic. I don't see anything in the datasheet that suggests some limit on the CLKOUT relative to input voltage. The part looks pretty plug and play, and the tech for producing these clock signals for sync is pretty mature, so I'm sure the part works fine IRL.

    For now, for simulation, I would try your suggestion of trying with two external out of phase clocks. You could try the LTC6909 built for this purpose or simply apply a PWM signal to both sync pins. I may give it a shot.

    mike

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.