| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Met after 8 hours |
emrecangidik EarlJohn MStokowski |
Open |
LTC6902
Production
The LTC6902 is a precision, low power and easy-to-use oscillator that provides multiphase outputs in a small package. The oscillator frequency is set by...
Datasheet
LTC6902 on Analog.com
LTspice
Production
LTspice® is a powerful, fast, and free SPICE simulator software, schematic capture and waveform viewer with enhancements and models for improving the simulation...
LTspice on Analog.com
Dear LTspice Team,
The LTC6902 model is not working as expected in the LTSpice version 24.0.3. For some reason, OUT2 doesn’t seem to phase shift, and startup behavior is quite different.
Expected behavior should be like below:
OUT1: 0°
OUT2: 90°
OUT3: 180°
OUT4: 270°
This model is working correctly in the LTSpice XVII Version 17.0.37.0.

working model.


The simulation results of the same schematic with LTSpice 24.0.3:

unexpected behavior.
Hi Earl,
Is there any news on this issue?
Thanks,
Emrecan
Hi Earl,
Is there any news on this issue?
Thanks,
Emrecan
Hi emrecangidik ,
This had been already addressed about 3 weeks ago.
It should already appear on the LTspice model change log.
Best Regards,
Earl