Post Go back to editing

modeling differential passive filter in LTSpice

Category: Hardware
Product Number: AD8138

I'm trying to model a discrete component filter being driven by an AD8138, through the filter, and into an LTC2153-14 ADC. I don't have those active components in the sim, just the discrete components, along with their parasitics. While the filter shape is what I expect, it peaks at greater than 0dB no matter how I try to model it, and that is nonsensical. Is there a recommended way to drive a circuit like this differentially and then retrieve the output, also differentially?PN8303_BPF.asc

Parents Reply Children
  • Hi Earl,

    L4 was an error and we are considering removing it. How can a passive filter provide gain boost above 0dB? I understand that the amplitude is actually dBV, but with unity input it should come out in the wash. Is this performance real, or am I missing a gain factor in the use ot the voltage-dependent voltage source? A passive circuit with gain above 0dB is nonsensical, making me have difficulty believing the results. Any thoughts?

    Mark

  • If the source impedance does not match the filter impedance, does not match the output load impedance then Yes there can be higher voltage amplitude at the output. The output power equals the input power (assuming no resistive loss in filter) but the voltages and currents won't match.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.