I downloaded the Spice model of MAX5078 from Analog Device documents, I automatically generated the symbol using LTspice sukckt and created a simple schematic for the simulation but the simulation doesn't work. I ask for support.2313.Test 5078.asc
MAX5078
Production
The MAX5078A/MAX5078B high-speed MOSFET drivers source and sink up to 4A peak current. These devices feature a fast 20ns propagation delay and 20ns rise...
Datasheet
MAX5078 on Analog.com
I downloaded the Spice model of MAX5078 from Analog Device documents, I automatically generated the symbol using LTspice sukckt and created a simple schematic for the simulation but the simulation doesn't work. I ask for support.2313.Test 5078.asc
EarlJohn - Moved from Power Management to LTspice. Post date updated from Tuesday, July 23, 2024 2:21 PM UTC to Wednesday, July 24, 2024 12:58 PM UTC to reflect the move.
EarlJohn - Moved from Power Management to LTspice. Post date updated from Wednesday, July 24, 2024 12:58 PM UTC to Wednesday, July 24, 2024 12:58 PM UTC to reflect the move.
HI lisian ,
Can you share with us the Symbol File (.asy) and Model File you used?
Best Regards,
Earl
lisian, please upload your symbol (.ASY file) too. Apparently you edited your symbol file because the auto-generated symbol does not fit in your schematic.
Andy
I uploaded both symbol (MAX5078 symbol.zip) and model file (max5078 Model.zip, original Analog model). I edited the symbol only to change the size and add the name of the pins as text.
Thank you, and sorry. I missed that there were two files on the same line.
Andy
No problem, I'm happy to have help!
Hi Andy, were you able to find out why the model doesn't seem to work? Thanks, Antonio
lisian,
I'm sorry but I did not yet. I was too busy. Last night I started looking at it again but had to stop.
Did you say what didn't work? Was there an error message, or just the wrong waveforms?
Andy
The simulation does not show any output signal from the MAX5078. At the end of the simulation the following Log message appears:
Antonio