Post Go back to editing

LTSpice example simulation

Category: Datasheet/Specs
Product Number: LT8333

Hi, I am currently designing a USB 5V to +/-18V for use with linear amplifier circuits.  The LTSpice provides good information on circuit behaviour except when I query the chip SW current it reports back with values up to 40A. This is 10x higher than I expected, given its rated as a 4A switch. The rest of the simulation seems OK with inductor current and voltage within the anticipated range. What have I missed ? Any help gratefully received.

Thread Notes

Parents Reply Children
  • Hi  ,

    These switch edge spikes might be real real at about 300ps in width. Not much energy in there. They do seem "real" in the simulation, not just numerical artifacts. I'll look into if this is modeled correctly. Anyway, the 20A over 100s of ps is pretty low when integrated, so overall operation probably close to real real?

    Anyway, I ran a sim with no max time step and saved the state at 3ms. And then loaded the state and ran a tran to 3.0004ms with a 10ps timestep max:

    Looks like a real spike, again, at under 400ps is much less than 8µAs I think.

    mike