Hello,
I am trying to design a circuit with the AD8130 that takes in a differential pair of high frequency clock signals (Each +/- 2.5V amplitude and 50MHz frequency) and outputs a single ended clock pulse of 5V amplitude and 50MHz frequency. I realize that I can do this with a logic translator, but I specifically want to do it with an amplifier.
According to my calculations I would need an op amp with GBW sufficient for 50MHz (AD8130 is 270MHz) and of slew rate of 786 V/microsecond or better.
I am following the circuit configuration in the datasheet (below)

Here is my LTSpice circuit (apologies forgot to label terminals):

So if my circuit follows correct what is in the datasheet, Rf and Rg (defined in datasheet) are both 1k ohm, so Vout = Vin(1+Rf/Rg) = 2* Vin.
However my output looks completely off (output signal is Red) :

So finally, my questions are:
1. Is the op-amp I selected suited for this task? If not, do you have suggestions that are better suited for this?
2. What is wrong with my circuit? Why am i getting such an output? Isn't the AD8130 rated for this task? How should I fix my circuit?
3. What is the gain I would need to configure for this task? (I assumed it was 2 but maybe I am wrong).
Please let me know about this. Any help would be greatly appreciated.
Thank you!
J.C.