Post Go back to editing

ADM708 LTSpice model doesn't work

Category: Hardware
Product Number: ADM708

Hello I would want to simulate a circuit based on ADM708 in LTSpice.

My first attempt was to use the furnished example circuit.

But it seems that the model doesn't work as expected.

The example circuit is (note the useless R1 and WDO net !)

Resulting simulation gives

But it should gives (if I'm not wrong !)

Could somebody help me ?

Thanks a lot in advance,

Pascal

Thread Notes

Parents
  • Hi  ,

    The voltage threshold for this part is 4.4V. Only upon reaching that threshold, it will start counting the reset timeout period of 200ms before the Vreset de-asserts.
    What you are seeing right now, the VCC only reaches until 4.5V before it ramps down so the time to de-assert the Vreset to 4.5V is not enough. 
    Try to increase the VCC to 5V and remain on that value, with that you could see that the Vreset will de-assert. Or instead of immediately ramping down from 4.5V, put enough time to stabilize the VCC before you ramp it down.

    Regards,
    Bianca

Reply
  • Hi  ,

    The voltage threshold for this part is 4.4V. Only upon reaching that threshold, it will start counting the reset timeout period of 200ms before the Vreset de-asserts.
    What you are seeing right now, the VCC only reaches until 4.5V before it ramps down so the time to de-assert the Vreset to 4.5V is not enough. 
    Try to increase the VCC to 5V and remain on that value, with that you could see that the Vreset will de-assert. Or instead of immediately ramping down from 4.5V, put enough time to stabilize the VCC before you ramp it down.

    Regards,
    Bianca

Children
No Data