Hi,
I would like a LTSpice model for MAX17291B and ADG1401BCPZ please.
Thanks,
Soumendu
MAX17291B
Recommended for New Designs
The MAX17291B is a low quiescent current boost (step-up) DC-DC converter with a 100mA peak inductor current limit and True Shutdown. True Shutdown disconnects...
Datasheet
MAX17291B on Analog.com
Hi,
I would like a LTSpice model for MAX17291B and ADG1401BCPZ please.
Thanks,
Soumendu
EarlJohn - Moved from Power Management to LTspice. Post date updated from Monday, May 20, 2024 7:47 PM UTC to Monday, May 20, 2024 10:04 PM UTC to reflect the move.
Hi Soumendu ,
The ADG1401 model ships with LTspice. Make sure you are using the latest version available at analog.com/ltspice.

The MAX17291B model is not yet available.
mike
Hi Mike,
Thank you - I was able to get the ADG1401 in my circuit. Is there a chance I can get a model for MAX17291 created? If not, what is the closest boost converter I can use for 12V, 100mA load setting that has an existing model in LTSpice? Thank you for your help!
Regards, Soumendu
Hi Mike,
Thank you - I was able to get the ADG1401 in my circuit. Is there a chance I can get a model for MAX17291 created? If not, what is the closest boost converter I can use for 12V, 100mA load setting that has an existing model in LTSpice? Thank you for your help!
Regards, Soumendu
Hi Soumendu ,
You would want to contact the applications engineer for this part or your local FAE if you require a model. As far as looking for alternates, the best way is to check the parametric table for internal switch boosts for similar parts. Here is the table sorted for 12V outputs. You can assume most of the LT or LTC prefix parts have LTspice models. For instance, the LTC3124 or LT3582. Some of the MAX and ADP prefix converters will have models. For any of the parts in the parametric table, click on the part name to go to its landing page. Once there, scroll down to Tools and Simulations. If there is a model, it should be listed here, and will be loaded with the latest version of LTspice.

I see you are on LTspice 17. The latest Windows version is LTspice 24.x; Mac is 17.x.
Latest versions of LTspice are available here.
mike