Post Go back to editing

Need LTSpice Model

Category: Software
Product Number: MAX17291B
Software Version: LTSpice 17

Hi,

I would like a LTSpice model for MAX17291B and ADG1401BCPZ please. 

Thanks,

Soumendu

Thread Notes

Parents Reply Children
  • Hi Mike,

    Thank you - I was able to get the ADG1401 in my circuit. Is there a chance I can get a model for MAX17291 created? If not, what is the closest boost converter I can use for 12V, 100mA load setting that has an existing model in LTSpice? Thank you for your help!

    Regards, Soumendu

  • Hi  ,

    You would want to contact the applications engineer for this part or your local FAE if you require a model. As far as looking for alternates, the best way is to check the parametric table for internal switch boosts for similar parts. Here is the table sorted for 12V outputs. You can assume most of the LT or LTC prefix parts have LTspice models. For instance, the LTC3124 or LT3582. Some of the MAX and ADP prefix converters will have models. For any of the parts in the parametric table, click on the part name to go to its landing page. Once there, scroll down to Tools and Simulations. If there is a model, it should be listed here, and will be loaded with the latest version of LTspice. 

    I see you are on LTspice 17. The latest Windows version is LTspice 24.x; Mac is 17.x.

    Latest versions of LTspice are available here.

    mike