LT8708
Recommended for New Designs
The LT8708 is a high performance buck-boost switching regulator controller that operates from an input voltage that can be above, below or equal to the...
Datasheet
LT8708 on Analog.com
Hi. Is there any way to simulate the lt8708 ic in ac analysis in LTSpice? A requirement of mine is compensation and when using ac analysis there are no results. I also tried making a simplis model but there are not enough information in the datasheet to create an equivalent model.
MStokowski - Moved from Power Management to LTspice. Post date updated from Monday, May 20, 2024 8:45 AM UTC to Tuesday, May 21, 2024 6:11 PM UTC to reflect the move.
Hi kennethaei ,
Yes, there is. The LT8708 model and example circuit ships with LTspice. Create a new schematic. Choose Edit > Component > [type LT8708 in the search field]. Select the LT8708 or LT8708-1, and then click either Place or Open Example Circuit. I'm attaching the example files here, too.
4135.LT8708.asc2043.LT8708-1.asc
mike
Hi kennethaei ,
Yes, there is. The LT8708 model and example circuit ships with LTspice. Create a new schematic. Choose Edit > Component > [type LT8708 in the search field]. Select the LT8708 or LT8708-1, and then click either Place or Open Example Circuit. I'm attaching the example files here, too.
4135.LT8708.asc2043.LT8708-1.asc
mike