Hello everyone,
I am trying to model a circuit with the LM7171 opamp from TI. I have a very small, high frequency current signal (around 1 microA, 300 kHz) that I want to convert to a voltage signal and amplify. The simulation results from LTspice don't make sense. Why is my response centered at -14.992 V? The voltage signal is not amplified either. I am using a MacBook and I made sure the number of pins in the .lib file match the pins in the symbol (1 to 5, +In, -In, +, -, out).
Would someone be able to help lead me in the right direction or tell me where I am going wrong?
Thank you for your help in advance - it is much appreciated.
Moved to LTspice forum from Amps. Expanded subject.
[edited by: MStokowski at 5:08 PM (GMT -4) on 12 Mar 2024]