I need to be able to set the solver to alternate for a particular simulation This is important because doing it from teh control panel affects all sims - which I do not want.
Looked all over the internet / LTwiki.
What is the spice .OPTION directive to do this in the schematic?
Dear Laudio ,
That is currently not possible, but such an option is in preparation for an upcoming release. Until then, you can control the solver choice via command line parameters. (See help file.)
Best regards,
Mathias
Any update on this? I have downloaded LTspice 24.0.12 but this doesn't seem to be an option still.
Will come in LTspice 24.1.
Thanks for the quick reply Mathias, looking forward to it!