I can not reach 240ua value in the following ac-lr circuit
The inductor has 33mH inductance and 65ohm resistance values.
Resistor has 10ohm resistance value.
They are connected in series with 0.5(vmax) and 10000 hertz ac source.
impedance value is about 2074.807 and Imax value should be about 240ua,
I couldn't reach that value, ltspice plotting diagram always give around 220ua.