Hello,
it seems that activating shutdown on these OpAmp models does not switch the outputs to tristate mode as described in the datasheet, but connects them to GND instead.
This can be demonstrated by driving the output with an external voltage source (via a resistor).
When shutdown is activated, the output is held at 0 V, even though no other pin of the opamp is connected to GND.
LTSpice test schematic attached.
ADA4099-1-Shutdown-Test.asc