LTC6752
Recommended for New Designs
The LTC6752 is a family of very high speed comparators capable of supporting toggle rates up to 280MHz. These comparators exhibit low propagation delays...
Datasheet
LTC6752 on Analog.com
Hi, I simulate with below schematic. LTC6752 is powered by ±2.5V.
The input signal V3 is 1V AC amplitude with 1V DC bias sinusoidal waveform.
We intend to use capacitor to isolate the DC bias and feed only AC waveform to LTC6752 IN+, but the simulation waveform shows that the DC bias is not removed by the cap.
Below V(s1) is the original 1V AC amplitude with 1V DC bias sinusoidal waveform.
V(s2) is the waveform after capacitor C2.
Why DC is not removed?
And with the same circuit with ADA4522, the DC bias could be removed. (See picture below, right side).

My simulation file is as below:
Hello,
your circuit ignores the input bias current, which is required at the input of the opamp/comparator. This is a DC-current, and since your coupling capacitor does not allow DC-currents, the input of the opamp/comparator will drift over time.
The simulation looks better for the ADA4522, because its input bias current is much smaller than the input bias current of LTC6752 (in the 100pA range instead of the 1µA range). Due to this huge difference the drift of the input voltage for ADA4522 is 10000 times slower than for the LTC6752 and cannot be recognized on the simulated time scale. But in the real circuit it will appear, both circuits will not work as intended in reality.
For a working AC-coupling you have to add some resistor after the coupling capacitor. This resistor will carry the input bias current, and so it will determine the midlevel at the amplifier input. If you take e.g. a 100k resistor after C2 to GND, the midlevel at the input of the LT6752 will typically be in the range of ~100mV (~1µA*100kOhm).
best regards
Achim