Post Go back to editing

LTC3729 model does not discharge RUN/SS cap

Category: Software
Product Number: LTC3729
Software Version: 17.1.10

The LTC3729 datasheet states that the if the output voltage falls below 70% then the RUN/SS pin will start discharge the softstart cap.  I do not see this occur in the model when I apply a heavy step load to the output.  The Run/SS pin never discharges even though I'm in a current limit and voltage has folded back well below 70%.  I'm trying to better understand how this behaves to balance softstart time vs not latching off, but the model does not appear to work properly.

9151_5V_30A_3729_2phase.asc

Parents
  • Hello,

    I have confirmed that the RUN/SS pin in the LTC3729 LTspice model does not work correctly in regards to the over-current latch-off. The RUN/SS pin of the actual LTC3729 circuit does work as described in the data sheet. If the supply requires over-current latch-off, then the LTC3729 will provide this function. If not required, then over-ride the RUN/SS pin with a 5uA pullup as described in the data sheet.  

    Note, regardless of which method is used, drive the RUN//SS pin with an external UVLO comparator or logic to reset it when Vin goes  low. This is shown below.

    Best regards, 

    Mike

Reply
  • Hello,

    I have confirmed that the RUN/SS pin in the LTC3729 LTspice model does not work correctly in regards to the over-current latch-off. The RUN/SS pin of the actual LTC3729 circuit does work as described in the data sheet. If the supply requires over-current latch-off, then the LTC3729 will provide this function. If not required, then over-ride the RUN/SS pin with a 5uA pullup as described in the data sheet.  

    Note, regardless of which method is used, drive the RUN//SS pin with an external UVLO comparator or logic to reset it when Vin goes  low. This is shown below.

    Best regards, 

    Mike

Children
No Data