Post Go back to editing

Ltspice 17.1.9 symbols problem

Category: Software
Product Number: ltspice
Software Version: 17.1.9 (x64)

I downloaded LTspice version 17.1.9 and installed it on Windows 10 machine.

I found a problem with some symbols. ind, ind2 for example and apparently the ones with arcs.

Symbols do not appear as they always have.

when i rotate the symbol and zoom to fit entire schematic disappears and nothing is displayed.

The same thing happens if I insert the symbol LED it is not even displayed in the preview window.

Regards

Parents Reply Children
  • Hi  ,

    Thank you for raising this issue. Have you tried reopening the LTspice application? I have a newly installed LTspice version17.1.9 but I am not experiencing the same issue.

    Regards,

     

  • Hi,

    I downloaded a new LTspice on 5 july and reinstalled again. Same problem.

    1a) Start new LTspice session.

    2a) open a new project

    3a) choice inductor symbol from upper bar and put on sheet.

    4a) rotate it

    5a) click "zoom to fit" button, every thinks disappear.

    Try another think

    1b) create a new poroject

    2b) choice Led device (preview is missing)

    3b) install it on sheet. (symbol is not complete)

    4b) click "zoom to fit" button, every thinks disappear as before.

     

    Note component are still present non project, it is only a display problem. If a right click on the empty sheet and click "view -> SPICE Netlist" I can see it, components are present.

    Regards

    Giovanni

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.