Post Go back to editing

LTSpice 17.1 does not simulate, "stalls" but 17.0 does simulate

Category: Software
Product Number: LTSpice
Software Version: 17.1.8

I recently installed LTSpice 17.1.8 and tried to simulate a circuit that worked fine with LTSpice 17.0.36.0, but it stalls out at ~165ms and never completes.  I did a compare of the Control Panel parameters and do not notice any differences. I'm not sure why the new version does not work with my circuit.  I have attached the schematic file and the log file.  I tried on 2 different W10 machines  with the same result.

Of note, he default parts library must have changes, because D1 (BAS40HM) is no longer in the library.  I used BAS40HY and also added BAS40HM, but nether changes made a diffrence. 

Circuit: * S:\ENGINEERING\Technical Data\Electronics & Software\french\My Stuff\LTspice circuits\LTC7804_24Vsupply20230410.asc

Warning: Multiple definitions of model "mysw" Type: Switch
C1: both pins shorted together -- ignoring.
L6: both pins shorted together -- ignoring.
C18: both pins shorted together -- ignoring.
C19: both pins shorted together -- ignoring.
C12: Increased Cpar to 1e-010
WARNING: Node N012 is floating.
WARNING: Node N005 is floating.

Direct Newton iteration failed to find .op point.  (Use ".option noopiter" to skip.)
Starting Gmin stepping
Gmin = 10
Gmin = 1.07374
Gmin = 0.115292
Gmin = 0.0123794
Gmin = 0.00132923
Gmin = 0.000142725
vernier = 0.5
Gmin = 2.39452e-005
vernier = 0.25
vernier = 0.125
vernier = 0.0625
vernier = 0.03125
vernier = 0.015625
vernier = 0.0078125
vernier = 0.00390625
vernier = 0.00195313
vernier = 0.000976563
vernier = 0.000488281
Gmin = 2.39452e-005
Gmin = 0
Gmin stepping failed

Starting source stepping with srcstepmethod=0
Source Step = 3.0303%
Source Step = 6.82706%
Source Step = 6.85665%
Source Step = 6.88625%
Source Step = 6.91584%
Source Step = 6.94543%
vernier = 0.00146484
Source Step = 6.97798%
Source Step = 7.02237%
Source Step = 7.06676%
Source Step = 7.11115%
Source Step = 7.15554%
vernier = 0.00219727
Source Step = 7.20215%
Source Step = 7.26873%
Source Step = 7.33532%
Source Step = 7.4019%
Source Step = 7.46848%
Source Step = 7.53507%
vernier = 0.0032959
Source Step = 7.60498%
Source Step = 7.70486%
Source Step = 7.80473%
Source Step = 7.90461%
Source Step = 8.00448%
Source Step = 8.10436%
vernier = 0.00494385
Source Step = 8.25417%
Source Step = 8.40399%
Source Step = 8.5538%
Source Step = 8.70361%
Source Step = 8.85343%
vernier = 0.00741577
Source Step = 9.07066%
Source Step = 9.29538%
Source Step = 9.5201%
Source Step = 9.74482%
Source Step = 9.96954%
vernier = 0.0111237
Source Step = 10.2841%
Source Step = 10.6212%
Source Step = 10.9583%
Source Step = 11.2954%
Source Step = 11.6325%
vernier = 0.0166855
Source Step = 12.0875%
Source Step = 12.5931%
Source Step = 13.0988%
Source Step = 13.6044%
Source Step = 14.11%
vernier = 0.0250282
Source Step = 14.7673%
Source Step = 15.5257%
Source Step = 16.2842%
Source Step = 17.0426%
Source Step = 17.801%
vernier = 0.0375423
Source Step = 18.7491%
Source Step = 19.8867%
Source Step = 21.0244%
Source Step = 22.162%
Source Step = 23.2997%
vernier = 0.0563135
Source Step = 24.6648%
Source Step = 26.3713%
Source Step = 28.0778%
Source Step = 29.7843%
Source Step = 31.4907%
vernier = 0.0844703
Source Step = 33.4532%
Source Step = 36.0129%
Source Step = 38.5726%
Source Step = 41.1323%
Source Step = 43.692%
vernier = 0.126705
Source Step = 46.5077%
Source Step = 50.3472%
Source Step = 54.1868%
Source Step = 58.0263%
Source Step = 61.8659%
vernier = 0.190058
Source Step = 65.8974%
Source Step = 71.6568%
Starting source stepping with srcstepmethod=1
Could not converge to DC with sources off!
Pseudo Transient failed in finding the operating point at 0 s.
Trouble finding operating point....skipping operating point for Transient analysis.
Ignoring empty pin current: Ix(u1:3)
Ignoring empty pin current: Ix(u1:8)
Ignoring empty pin current: Ix(u1:9)
Ignoring empty pin current: Ix(u1:10)
Ignoring empty pin current: Ix(u1:11)
Ignoring empty pin current: Ix(u1:12)
Ignoring empty pin current: Ix(u1:13)
Ignoring empty pin current: Ix(u1:14)
Ignoring empty pin current: Ix(u1:15)
Ignoring empty pin current: Ix(u1:16)
Ignoring empty pin current: Ix(u1:17)
Ignoring empty pin current: Ix(u1:18)
Ignoring empty pin current: Ix(u1:21)
Ignoring empty pin current: Ix(u1:27)
Ignoring empty pin current: Ix(u1:28)
Changing Tseed to 9.76563e-011
to 1.95313e-010
Heightened Def Con from 0.000282691 to 0.000282695
Heightened Def Con from 0.000292388 to 0.000292389
Heightened Def Con from 0.000353001 to 0.000353005
Heightened Def Con from 0.000403906 to 0.000403906
Heightened Def Con from 0.000452347 to 0.000452351
Heightened Def Con from 0.000687496 to 0.0006875
Heightened Def Con from 0.000728729 to 0.000728733
Heightened Def Con from 0.000784467 to 0.000784471
Heightened Def Con from 0.000786883 to 0.000786883
Heightened Def Con from 0.000837799 to 0.000837803
Heightened Def Con from 0.000849929 to 0.000849933
Heightened Def Con from 0.000886252 to 0.000886256
Heightened Def Con from 0.000929881 to 0.000929885

Date: Fri Apr 28 10:07:52 2023
Total elapsed time: 37.924 seconds.

tnom = 27
temp = 27
method = Gear
totiter = 1481448
traniter = 1447790
tranpoints = 429766
accept = 343511
rejected = 86478
matrix size = 140
fillins = 35
solver = Normal
Thread vector: 16.5/11.5[6] 6.0/7.5[1] 2.1/3.4[1] 0.3/3.0[1]  2592/500
Matrix Compiler1: 5.39 KB object code size  2.2/1.2/[0.6]
Matrix Compiler2: 8.62 KB object code size  1.3/2.7/[0.7]

LTC7804_24Vsupply20230410.asc

Top Replies

  • Hi  ,

    There are a lot of changes made to improve in LTspice 17.1.x from 17.0.x. Unfortunately, due to the existing bugs/issues from the old version, the models developed using that version is…

  • Hi  ,

    There are a lot of changes made to improve in LTspice 17.1.x from 17.0.x. Unfortunately, due to the existing bugs/issues from the old version, the models developed using that version is made such that it will avoid or have a workaround not to trigger those bugs/issues. With the release of the 17.1.x, those work arounds may or may not cause issues. This is probably what cause your problem.

    I will report this issue to the part owner and them checked the model of LTC7804. 

    I am quite curious though why do you need to run your simulation for 165ms transient time, I don't see any event from your schematic that will change at that point like dynamic loading or line distortion. Do you mean 165us?

    I suggest you use the old version for now while we fix the problem with this model. Both LTspiceXVII (17.0.x) and LTspice (17.1.x) can exist as a separate application on your machine. so there should be any problem.

    just keep in mind that 17.0.x will no longer update its library. thus when this item is resolved, only 17.1.x will get updated.

    Thank you.

    Regards,

      

  • Hi PaulDaria,

    Thank you for the response.  Yes, I meant say 165µs, sorry about that.

    Well, I restarted my computer this Monday AM (probably the first time since the install) and now the simulation works like the older version.  I would consider this resolved. The only difference is with D1, the BAS40HY is not in the new version's (17.1) library.  Let me know if you need any more information.

    Thanks!