Post Go back to editing

LTspice 17.1 crashes, where as spice 17.0 solves the same simple .op analyses

Category: Software
Product Number: LTspice 17.1 .8
Software Version: LTspice 17.1.8 x64 running on windows 10

Dear ADI

I noticed that some of my simulations made in LTspice 17.0.36, do not work anymore in LTspice 17.1.8.

Al of a sudden it is 'raining' singular martix errors ( if you solve one it will find another) in Spice 17.1.8 when I start the simulation, where the simulation runs fine in 17.0.36. without errors.

What has changed in LTSpice?

I did some investigation, because it seems to happen with conductors with actual .model files attactched to them.

If you create the following simple schematic a single diode with anode floating and only run an operating point analyses; LTspice 17.1.8 will start analysis, completely freezes and than after 15 seconds or so LTspice crahses and closes the program.

 

 If you start the same analysis in Spice 17.0.36 . It wil solve it without any problem.

Se result here:

 I know it is not wise to have floating nodes in the circuit., but it is a simple way to show that LTspice 17.1.8 is doing something different than LT Spice 17.0.36 and is less stable operating.

A colleagues has run the same schematic on his PC and it had same result: LTspice 17.1.8 crashes.

(If you connect a capacitor from anode to ground ( value can be anything 1fF will do) . LTspice 17.1.8. will find a solution for the operating point

What has made LTspice 17.1.8 more sensitive ?

Kind regards

Ewold

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.