Post Go back to editing

Different results for FRA using LTpowerCAD and LTspice

Category: Software

1805.FRA.zip

Hello

I have a different results for LT8643S based step-down converter.

LTpowerCAD report closed loop bandwith 100kHz, LTspice 130kHz.
Which of them can be trusted?


See attachment, please.

Anyway... LTspice FRA settings is very poorly documented, I can not find any application notes or other sourses.

Only single basic and very short information available at

ez.analog.com/.../generate-a-bode-plot-for-an-smps-in-ltspice-17-1



NA
[edited by: Levandovsky at 10:43 AM (GMT -4) on 4 Apr 2023]

Top Replies

    •  Analog Employees 
    May 7, 2023 in reply to John Kevin +1 verified

    Hi ,

    Please be advised that the updated model for LT8643S is now available in the library. Please sync your library by going to Tool>Update components

    This result matches the result from LTpowerCAD…

Parents Reply Children
  • Hi ,

    We are on some finishing work to update the LT8643S model.
    We are now able to match the LTpowerCAD gain/phase plot.



    We will also be updating the models for the LT8608S and LT8390.

    For your question:LTpowerCAD vs. LTspice. Which of them can be trusted?

    LTpowerCAD simulation results have been demonstrated to be matching actual hardware test results of various ADI parts.
    The new LTspice FRA tool is also a good tool, well-designed to make measurements following the industry-accepted control loop theory.
    It just so happened that the model you encountered, the LT8643S has a missing internal parameter that affected its results in the frequency domain analysis. Nonetheless, the LT8643S model is still representing the actual device in time-domain analysis.

  • Hi ,

    Please be advised that the updated model for LT8643S is now available in the library. Please sync your library by going to Tool>Update components

    This result matches the result from LTpowerCAD.