Post Go back to editing

Different results for FRA using LTpowerCAD and LTspice, Specifically LT8643S and LT8390

Category: Software

1805.FRA.zip

Hello

I have a different results for LT8643S based step-down converter.

LTpowerCAD report closed loop bandwith 100kHz, LTspice 130kHz.
Which of them can be trusted?


See attachment, please.

Anyway... LTspice FRA settings is very poorly documented, I can not find any application notes or other sourses.

Only single basic and very short information available at

ez.analog.com/.../generate-a-bode-plot-for-an-smps-in-ltspice-17-1



Added LT8390 to keywords. Expanded subject.
[edited by: MStokowski at 8:39 PM (GMT -4) on 12 Mar 2024]
Parents
  • Hi  ,

    You can find more information about the FRA feature using the help file. Just type in FRA and all related topic will show up.

    FRA is a new feature of LTspice and thus app notes about this feature are still limited.

    with regards to the difference between LTpowerCAD and LTspice result. It depends, LTpowerCAD is limited to CCM mode of operation. also, it can be likely that there is a bug on the LTspice model.

    What I can do on the other hand is to consult the part owner and let them answer the question for you.

    Thank you.

    Regards,

     

Reply
  • Hi  ,

    You can find more information about the FRA feature using the help file. Just type in FRA and all related topic will show up.

    FRA is a new feature of LTspice and thus app notes about this feature are still limited.

    with regards to the difference between LTpowerCAD and LTspice result. It depends, LTpowerCAD is limited to CCM mode of operation. also, it can be likely that there is a bug on the LTspice model.

    What I can do on the other hand is to consult the part owner and let them answer the question for you.

    Thank you.

    Regards,

     

Children