Post Go back to editing

LTC2953-1 deasserts EN when it shouldn't

Category: Software
Product Number: LTspice LTC2953-1 Macromodel test fixture

Hi,

I think I found an error on the provided LTspice LTC2953-1  Macromodel test fixture. At t=6s, the PB input goes low and 500 ms later, high, simulating the pressing down of a pushbutton. Based on Figure 2 from the datasheet, as the time that the pushbutton remains in the "pressed-down" state is smaller than t_PD(min) + t_PDT (64 ms + 6.4s), the turn-off sequence should be aborted, and therefore the EN must remain asserted. This is not the case, as evidenced in the attached screenshot:

Could you please clarify whether this is indeed an error or not?

Thanks

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.